Connect different data sources to the platform and store the data for analysis and decision making.
Data spread across the enterprise and isolated in silos makes it difficult to identify issues impacting asset availability. With Plantweb Optics, an asset performance platform for managing enterprise asset health, data is combined from multiple applications into asset-centric information to deliver persona-based alerts and KPIs.
Plantweb Optics has real-time automated data collection from assets within the plant funneled into diagnostics and analytics platforms to help visualize, analyze, and predict performance. With this actionable data, plant service and maintenance is seamless with CMMS integrations and workflows. This platform makes staying on top of asset health in the plant easier than ever before.
Plantweb Optics connects data from multiple applications into asset-centric information to deliver persona-based alerts and KPIs for production assets. These applications are used to monitor, analyze, diagnose, and repair rotating equipment, instruments, and valves for improved decision making.
Connect different data sources to the platform and store the data for analysis and decision making.
Provide a persona based visualization, notification, and analytical tools.
Enable collaborative engagement between personas and drive a closed loop work practice.
Plantweb Optics delivers native data connections that can automatically contextualize data with minimal configuration. With these connections comes the ability to monitor asset health and capture all asset parameters and properties. Due to the low level of configuration, you can immediately start seeing insights and driving actions.
Plantweb Optics Data Lake aggregates global operational data from across the enterprise to create a centralized storage repository that serves as the foundation for machine learning and analytics. It provides increased data visibility for unified, actionable information to empower faster decision-making and optimized operations.
Collecting information with AMS Device Manager helps avoid unnecessary downtime and prevents inefficient practices that eat away at your bottom line. Based on real-time condition data from your intelligent field devices, plant staff can respond fast and make informed decisions on whether to maintain or replace field devices.
Gathering data from AMS Machinery Manager enables you to understand the health of your rotating mechanical assets and plan for repairs rather than react to failures. Your facility can achieve increased availability and performance from production assets, rather than experience expensive downtime and costly repairs.
With the AMS Trex Device Communicator in hand, you can properly diagnose device issues in the field without the need for other specialized tools. Maintenance teams will experience significant savings in work hours and peace of mind knowing that problems will be fixed quickly and properly the first time.
Asset Source Interfaces are custom connections into Plantweb Optics that require no configuration and immediately start contextualizing the data. The Asset Source interfaces leverage Emerson's domain knowledge to automatically assign health to provide your team the information it needs to take action.
Plantweb Optics is able to provide real-time actionable information and insights about abnormal situations to improve operational performance. Also, using machine learning, artificial intelligence, and root-cause analyses, you can be proactive when maintaining your plant and intervene before assets are underperforming or require shut down.
View Plantweb Optics Analytics data which enables proactive decision making by detecting abnormal behaviors of processes and assets in real-time leveraging artificial intelligence and machine learning techniques.
Combine asset health data collected through Plantweb Insight which is engineered with first-principled analytics.
Plantweb Optics Augmented Reality overlays digital information on the physical world for increased productivity, safety, and insight. The result is a digitally connected workforce equipped to complete tasks more accurately and keep production running with fewer interruptions. This means lower operational costs, reduced downtime for maintenance and operational tasks, and increased safety.
The Plantweb Optics mobile application delivers relevant information to your mobile device of choice so you stay connected to what is going on in your facility. Plantweb Optics enables better collaboration by creating messages based on observations and analysis from the field and assigning workflow tasks. The mobile app can connect to multiple Plantweb Optics systems to allow users to view the status of the enterprise from a single app featuring a dashboard summary of KPIs tailored to the connected data sources.
Easily identify unhealthy assets and quickly understand the severity of an event with automatic health scores
Display a personalized list of assets that you want to closely monitor
See all unread system and user-generated messages regarding that asset
Easily track work notifications and work orders from open to closed status
View calibrations scheduled in AMS Device Manager Calibration Management
Identify routes that are scheduled in AMS Machinery Manager
Determine offline prediction units from AMS Machinery Manager
Track AMS Machinery Manager “serious” open case histories
Assets are mapped from Plantweb Optics to popular CMMS systems, like IBM Maximo and SAP, to create a closed loop of workflow across the enterprise.