Learn More

Emerson’s New Ultrasonic Generators Offer User-Friendly Digital Controls for Fast Setups and Precise Operation

​Branson GCX Ultrasonic Generator

The new Branson™ GCX Series ultrasonic cleaning generators precisely control the delivery of energy for precision cleaning systems.
High resolution image

Branson GCX Series enables more efficient power delivery for ultrasonic cleaning systems

DANBURY, Conn. (August 10, 2020) – Today Emerson introduced its new BransonTM GCX Series of ultrasonic generators, which combine user-friendly digital controls, advanced features and a more compact footprint to precisely control the delivery of ultrasonic energy for precision cleaning systems used in medical, electronic, automotive and other industries. 

The compact design of the Branson GCX Series generator is 15% smaller than that of its predecessor — the S8000 Series — and is built around a 5-inch color human-machine interface (HMI) touchscreen. The user-friendly HMI eliminates older analog push-button settings with a wider range of precise, digital settings. The GCX Series offers fully variable power control, enabling the user to vary cavitational intensity from 20% to 100%, and a power modulation mode that can automatically increase cleaning power fourfold. Sweep frequency mode can vary cavitation intensity to eliminate standing waves and reach even small or intricate part features. It replaces fixed “hi/low” sweep settings and enables users to select sweep bandwidths from 1% to 100%. 

The new GCX alarm display puts an end to time-consuming alarm-code lookups by displaying plain-text alarms on the HMI screen, prompting the user to select and review plain-language alarm information, troubleshooting tips and resolution procedures. The alarm system also includes a complete log of recent alarms, with all HMI text information available in multiple languages — English, Chinese and Japanese. Process monitoring is further simplified with a power-graphing display that continually tracks the generator’s power draw, enabling fast recognition of any sudden variations that could affect ultrasonic output or cleaning performance. Together, these features simplify monitoring and reduce the need for paper documentation and technical support calls.

“The GCX Series continues the superior performance and durability of the S8000 Series, while its new and more powerful controls, HMI and communications capabilities give users a far greater level of precision, control and information about the ultrasonic cleaning process,” said Nitin Phadnis, director of precision cleaning products for Emerson. “The GCX Series replaces the entire S8000 Series of more than 60 models, simplifying product selection while offering a new degree of user-friendly performance for ultrasonic cleaning operations.” 

The GCX Series also features enhanced RS-485 communications capabilities, which enable high-speed availability of setup and cleaning process data to programmable logic controllers (PLCs), servers or PCs for statistical process analysis. All GCX units can operate with individual tanks in a stand-alone configuration or integrate fully with the PLC controls common to OMNI, B Series Degreasers and other Branson ultrasonic cleaning systems.

For more information about the latest Branson welding solutions, visit Emerson.com/Branson.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson 
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.

Please enable JavaScript to use this website.